October 19, 2011
Half-Pitch 4-ch Transistor Photocouplers Offer Wider Creepage Distance and Higher Operating Temperatures
IRVINE Calif., — Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has announced the addition of the TLP290-4 (AC input) and TLP291-4 (DC input) to its family of optocouplers. Suitable for general purpose applications requiring isolation, including power supplies and motor controllers, the new optocouplers from Toshiba feature a quad configuration in a double - molded package and a wider creepage distance, improved performance and higher operating temperatures (110 degrees Celsius).
The Toshiba TLP290-4 and TLP291-4 both consist of a photo transistor that has been optically coupled to a gallium arsenide infrared emitting diode. The devices are housed in a low profile SO16 package, making for extremely small and thin couplers. TheTLP290-4 and TLP291-4 feature a wide operating temperature (Ta=-55 to 110 degrees Celsius), making them suitable for high-density surface mounting applications such as programmable controllers and hybrid ICs.
According to Joseph Tso, business development manager for Toshiba's optoelectronics discrete business unit , "This new family of quad couplers can be used in the same socket as our popular TLP280-4 and TLP281-4 series of optocouplers, offering higher performance and greater creepage distance for designs in which package height is of a lesser concern."
The Toshiba TLP290-4 and TLP291-4 are available now. The TLP290-4 is priced at $0.90 each in low quantities and the TLP291-4 is priced at $0.72 in low quantities.
Toshiba is a leading supplier in a number of discrete product categories, including power transistors, rectifiers and thyristors, LMOS logic, CMOS logic, photocouplers, Toslinks™, LEDs, small signal diodes and transistors. The company's discrete devices are designed to meet the growing demand for high-performance and lower voltages in today's wireless telecommunications and consumer electronics applications, while emphasizing its strength in the automotive and industrial markets.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs ), hard disk drives (HDDs), discrete devices, LCD displays, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2010 WW Semiconductor Revenue, April 2011). Toshiba was founded in 1875 and today has over 490 subsidiaries and affiliates, with 203,000 employees worldwide and annual sales of $77 billion. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
OPTO 11 622