November 2, 2011
Series Includes Industry's First Hot-Swap 2.5V CMOS Logic IC
IRVINE Calif., — Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has announced the addition of the TC74LCXZ and TC74LCXZA to its family of low-voltage CMOS logic ICs. The new ICs from Toshiba feature a built-in power-up/power-down HZ (high-impedance) function and can maintain output at high impedance when power supply voltages are in the range of 0 to 1.5V (TC74LCXZ Series) and 0 to 1.2V (TC74LCXZA Series). This function enables hot-swap applications when the main system is turned on. Both the 74LCXZ and 74LCXZA come in 3-State inverted and non-inverted buffer.
Hot-swap ICs manage inrush current during live insertion of cards in order to prevent system failures. Hot-swap applications include factory automation and network equipment.
The TC74LCXZ and TC74LCXZA Series can be used for 3.3V and 2.5V systems respectively, and theTC74LCXZA Series, in particular, is one of the industry's first hot-swap 2.5V CMOS logic ICs. In addition, this new series of ICs can achieve a reduction in consumption current for BiCMOS logic ICs.
Part Number | Function | Package | Number of Pins | Number of Circuits | Operating Supply Voltage (VCC, max) | Operating Supply Voltage (VCC, min) | Output Current (max) (mA | Propagation delay time (tpd/tpz) max |
TC74LCXZ240FK | Octal Bus Buffer (3-State, Inverted) | US20 | 20 | 8 | 3.6 V | 2.7 V | 36 at 3V | 6.5 ns at 3.3+-0.3V |
TC74LCXZ240FT | TSSOP20 | 20 | 8 | 3.6 V | 2.7 V | 36 at 3V | 6.5 ns at 3.3+-0.3V | |
TC74LCXZ244FK | Octal Bus Buffer (3-State) | US20 | 20 | 8 | 3.6 V | 2.7 V | 36 at 3V | 5.9 ns at 3.3+-0.3V |
TC74LCXZ244FT | TSSOP20 | 20 | 8 | 3.6 V | 2.7 V | 36 at 3V | 5.9 ns at 3.3+-0.3V | |
TC74LCXZA240FK | Octal Bus Buffer (3-State, Inverted) | US20 | 20 | 8 | 2.7 V | 2.3 V | 18 at 2.3V | 7.5 ns at 2.5+-0.2V |
TC74LCXZA240FT | TSSOP20 | 20 | 8 | 2.7 V | 2.3 V | 18 at 2.3V | 7.5 ns at 2.5+-0.2V | |
TC74LCXZA244FK | Octal Bus Buffer (3-State) | US20 | 20 | 8 | 2.7 V | 2.3 V | 18 at 2.3V | 7 ns at 2.5+-0.2V |
TC74LCXZA244FT | TSSOP20 | 20 | 8 | 2.7 V | 2.3 V | 18 at 2.3V | 7 ns at 2.5+-0.2V |
The Toshiba TC74LCXZ and TC74LCXZA are available now.
Toshiba is a leading supplier in a number of discrete product categories, including power transistors, rectifiers and thyristors, LMOS logic, CMOS logic, photocouplers, Toslinks™, LEDs, small signal diodes and transistors. The company's discrete devices are designed to meet the growing demand for high-performance and lower voltages in today's wireless telecommunications and consumer electronics applications, while emphasizing its strength in the automotive and industrial markets.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs ), hard disk drives (HDDs), discrete devices, LCD displays, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2010 WW Semiconductor Revenue, April 2011). Toshiba was founded in 1875 and today has over 490 subsidiaries and affiliates, with 203,000 employees worldwide and annual sales of $77 billion. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
LGSS 11 623