require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
September 25, 2012
Featuring Low Noise Output and the Industry's Highest Level of Drop-Out Voltage in an Ultra-Small Package
IRVINE, Calif., — Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the introduction of a new lineup of CMOS-LDO regulators for mobile devices. The new lineup features Toshiba's newly developed micro CMOS process and offers the highest level of drop-out voltage in the industry. The new regulators also achieve low noise output, low consumption current and excellent load transient response.
CMOS-LDO regulators have become the power management ICs of choice for mobile devices, as they enable a low profile, low supply current and low dropout. Toshiba's new TCR2EN, TCR2EE, TCR2EF, and TCR2DG series utilize a newly developed micro CMOS process, which helps the regulators to significantly improve the tradeoff between characteristics and size. Toshiba's TCR2DG is a 200mA output single LDO regulator which achieves a low-noise output of 18µVrms (2.5V output), excellent ripple rejection ratio 62dB at a high frequency (2.5V output, f = 10kHz), excellent responsibility under high-speed loads of ⊿ VOUT = ±65mV (IOUT = 1mA ⇔ 150mA, COUT = 1.0µF), and low drop-out characteristics of 80mV (2.5V output, IOUT = 100mA). By using an ultra-small (0.79mm x 0.79mm x 0.5mm) WCSP4 package, this LDO regulator is suitable for applications requiring high-density packaging, such as mobile devices.
In addition to overcurrent protection, output auto-discharge, and other basic functions, the new lineup of 200mA output LDO regulators control inrush current, making them suitable for a wide range of applications including mobile phones, portable audio players, notebook PCs, DSC/DVC, and other small mobile devices.
According to Talayeh Saderi, senior business development engineer for TAEC, "An ideal power management solution for mobile devices using battery power, CMOS LDOs provide space conscious designers with cost effective performance advantages - all while extending battery life."
TCR2EN Series
Lineup of TCR2EN Series (SDFN4, 0.8mm x 0.8mm x 0.38mm)
Part number | Output voltage |
TCR2EN12 | 1.2V |
TCR2EN18 | 1.8V |
TCR2EN28 | 2.8V |
TCR2EN29 | 2.9V |
TCR2EN30 | 3.0V |
TCR2EE and TCR2EF Series
Lineup of TCR2EE, TCR2EF Series
Part number | Output voltage | |
SOT553 (ESV) | SOT-25 (SMV) | |
TCR2EE10 | TCR2EF10 | 1.0V |
TCR2EE11 | TCR2EF11 | 1.1V |
TCR2EE12 | TCR2EF12 | 1.2V |
TCR2EE13 | TCR2EF13 | 1.3V |
TCR2EE18 | TCR2EF18 | 1.8V |
TCR2EE28 | TCR2EF28 | 2.8V |
TCR2EE30 | TCR2EF30 | 3.0V |
TCR2EE33 | TCR2EF33 | 3.3V |
Lineup of TCR2DG Series (WCSP4: 0.79x0.79x0.5mm)
Part number | Output voltage | Package |
TCR2DG12 | 1.2V | |
TCR2DG13 | 1.3V | |
TCR2DG15 | 1.5V | |
TCR2DG18 | 1.8V | |
TCR2DG25 | 2.5V | |
TCR2DG28 | 2.8V | |
TCR2DG30 | 3.0V | |
TCR2DG33 | 3.3V | |
TCR2DG36 | 3.6V |
Toshiba's lineup of CMOS-LDO regulators is currently available. For datasheets and samples, please contact your Toshiba representative.
* About Toshiba Corp. and TAEC
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2011 Worldwide Semiconductor Revenue, March, 2012). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
Editors Note: Images available for download from:
LGSS 12 646