Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Expands Its TransferJet™ Offering With New Products That Simplify Implementation of the Close Proximity Wireless Transfer Technology

October 1, 2012

Industry's smallest SDIO IC module1, and industry's first microSDIO card2 and USB adaptor3 drive adoption of TransferJet™ technology

TransferJet

SAN JOSE, Calif., — Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create break through designs, today announced three new additions to its products supporting the TransferJet™ close proximity wireless data transfer technology. The company will make available the industry's smallest TransferJet™ -enabled SDIO IC module, and the industry's first TransferJet ™ -enabled microSD IO card and TransferJet™ USB adaptor. These devices are designed to easily deploy and proliferate TransferJet™ technology for the high-speed transfer of large multimedia files between consumer electronics products through close proximity, or simply by touching two devices together.

"Toshiba applies its expertise in wireless technology to deliver a simple connection, high-speed wireless communication technology in its TransferJet™ products," said Andrew Burt, vice president of the Analog and Imaging Business Unit, System LSI Group at TAEC. "The company is stepping up to drive the adoption of the TransferJet™ technology by offering OEMs an easy and cost-effective way to implement this technology and capitalize on an emerging machine-to-machine wireless communications market."

Toshiba continues to leverage its advanced RF-CMOS LSI manufacturing technology and experience in high-frequency design and system integration to achieve the performance, compact size and integration benefits presented in its TransferJet™ products. The Toshiba TransferJet™ offering gives OEMs a quick path to implementation and builds up the eco-system infrastructure for this technology. End users will enjoy the extremely high-speed exchange of data and multimedia content on their TransferJet™ -enabled devices just by touching the devices together, without the inconvenience of going through a complex setup.

Industry's Smallest TransferJet™-Enabled SDIO IC Module (Part #TJM35420XLG)

Toshiba has created the industry's smallest TransferJet™ -enabled SDIO IC module that simplifies implementation and design challenges associated with compact consumer electronics products. The Toshiba TransferJet™ -enabled SDIO IC module is delivered in the industry's smallest configuration, 4.8 x 4.8 x 1.0 mm for a significant reduction in solution footprint. Toshiba applies its high-frequency design technique and system integration experience to minimize mounting footprint for smartphone and other portable device applications. The TransferJet™ -enabled SDIO IC module integrates the Toshiba TransferJet™ transceiver IC, RF components, and a crystal oscillator. A software development kit is available.  

Industry's First TransferJet™-Enabled microSDIO Card (Part #TJM35420USG)

Toshiba has developed the industry's first TransferJet™ -enabled microSDIO card that can be inserted into a variety of compact, portable products like smartphones and tablets to enable the technology. The TransferJet-enabled microSDIO card integrates a TransferJet™ tranceiver IC, a TransferJet™ coupler, RF components, and a crystal oscillator that makes TransferJet™ implementation quick and easy. A software development kit is available.  

Industry's First TransferJet™ USB Adaptor (Part #TJM35420UXG)

The Toshiba TransferJet ™ USB adaptor implements TransferJet™ communications easily, conveniently, and efficiently in larger consumer electronic products like notebooks, PCs and other digital gadgets . The TransferJet™ USB adaptor integrates a TransferJet™ transceiver IC, a TransferJet™ coupler, RF components, and a crystal oscillator making for simple implementation.

Availability

The Toshiba TransferJet ™ -enabled SDIO IC module begins sampling in the fourth quarter of 2012, with mass production beginning in the first quarter of 2013. The microSDIO card and the USB adaptor will be available in the first quarter of 2013. For more information please visit: http://www.toshiba.com/taec/support/techquestions/index.jsp.

About TransferJet™ Technology

The TransferJet™ technology enables close proximity wireless data transfer and is a standard promoted by the TransferJet™ Consortium whose membership consists of 45 companies (as of October 1, 2012), including Toshiba. TransferJet™ technology provides the simplest connection and ultra high-speed data transfer with low power consumption simply by selecting on the screen of a mobile device the data file to be transferred and "touching" the receiving device with the mobile device. Applications of TransferJet™ technology could expand to future digital signage application for large digital content download when combined with Near Field Communications (NFC) technology.

**About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs ), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan 's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2011 Worldwide Semiconductor Revenue, and March, 2012). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.

Note: TransferJet™ is a trademark licensed by the TransferJet™ consortium.

1Smallest as of Oct. 1, 2012

2First as of Oct. 1, 2012

3 First as of Oct. 1, 2012


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba's Handling Guide for Semiconductor Devices, or Toshiba Semiconductor Reliability Handbook. This information is available at www.toshiba.com/taec, or from your TAEC representative.

Editors Note: Reader inquiries please publish: Tech.Questions@taec.toshiba.com.

Photos available for download at Photo Gallery http://www.toshiba.com/taec/news/media_resources/news_mr_gallery.jsp http://www.toshiba.com/taec/news/images/gallery/wireless/tjet_lrg.jpg

WRLS 12 647

A new window will open