March 19, 2013
TK16A60W5, TK31J60W5, TK39J60W5 Improve Power Efficiency, Bring Industry Leading Level of RON•A
LONG BEACH, Calif., – This week at APEC 2013, Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, will introduce a new lineup of high-speed diodes (HSD): the TK16A60W5, TK31J60W5 and TK39J60W5. Based on Toshiba's fourth generation 600V system super junction MOSFET DTMOS IV series, the new lineup of HSDs improve power efficiency in switching power supplies, micro inverters, adaptors, and photovoltaic inverters. The new HSDs will be highlighted in Toshiba's booth #919 on the APEC show floor from March 17-21.
Using the latest single epitaxial process, this series has achieved the industry's leading level of RON•A (*) for high speed parasitic diodes. The TK16A60W5, TK31J60W5 and TK39J60W5 can further reduce loss by achieving a recovery time that is one third that of previous models, which significantly contributes to improvements in power efficiency.
Super junction MOSFETs offer ultra-low on resistance without power loss penalties . Using Toshiba's state-of-the-art single epitaxial process, the fourth generation super junction 600V DTMOS IV MOSFET series provides a 30 percent reduction in RON•A, a figure of merit (FOM) for MOSFETs, when compared to its predecessor, DTMOS III. A reduction in RON•A makes it possible to house lower RON chips in the same packages, helping to improve the efficiency and reduce the size of power supplies.
According to Norio Nakashima, business development specialist for TAEC, "Toshiba's DTMOS-IV technology uses a deep-trench process that narrows the lateral SJ pitch, leading to optimized overall performance. As a result, our new series gives customers a highly efficient switching device at an excellent cost-performance ratio."
Part Number | Absolute maximum rating VDSS (V) |
Absolute maximum rating ID (A) |
RDS(ON) Max (Ω) VGS=10V |
Qg Typ. (nC) |
Ciss Typ. (pF) |
trr Typ. (ns) |
Package |
TK16A60W5 | 600 | 15.8 | 0.23 | 43 | 1350 | 100 | TO-220SIS |
TK31J60W5 | 600 | 30.8 | 0.099 | 105 | 3000 | 135 | TO-3P(N) |
TK39J60W5 | 600 | 38.8 | 0.074 | 135 | 4100 | 150 | TO-3P(N) |
Toshiba's new 600V System Super Junction MOSFET DTMOS IV HSD Series is available now.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, MP3 players, cameras, medical devices, automotive electronics, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2011 Worldwide Semiconductor Revenue, March, 2012). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
*According to a survey by Toshiba. (As of December 2012)
Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
POWR 13 669