February 11, 2014
Significantly Help to Reduce Power Consumption for Industrial Devices
IRVINE, Calif., — Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has introduced a new family of low input current-type transistor output photocouplers that offer a high CTR (Current Transfer Ratio) at low input current. The TLP182, TLP183, TLP292, and TLP293 significantly contribute to a reduction in power consumption by reducing the LED current of the photocoupler.
Available in both SO4 (TLP292 and TLP293) and 4-pin SO6 (TLP182 and TLP183) packages, by employing Toshiba's original high-output LED, these products provide not only a high current transfer ratio at the conventional input current of 5mA, but also at the same current transfer ratio at the low LED current of 0.5mA. This makes it possible to minimize the current to the LED and therefore reduce power consumption. The TLP182, TLP183, TLP292, and TLP293 also support operation at up to an ambient temperature of 125°C, making them ideal for use in industrial devices such as PLCs and inverters, compact power supplies, AC line detection for household appliances, and other devices operating in extremely hot environments.
Characteristics | TLP182 | TLP183 | TLP292 | TLP293 | |
Package | 4-pin SO6 |
SO4 |
|||
Input type | AC | DC | AC | DC | |
Current transfer ratio (%) | @IF=5mA, VCE=5V | 50 to 600 | 50 to 600 | 50 to 600 | 50 to 600 |
@IF=0.5mA, VCE=5V | 50 to 600 | 50 to 600 | 50 to 600 | 50 to 600 | |
Topr (ºC) | -55 to 125 | -55 to 125 | -55 to 125 | -55 to 125 | |
BVs (Vrms) | 3750 | 3750 | 3750 | 3750 |
The new photocouplers are available now. Please contact your local Toshiba Sales Office for samples and pricing.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, advanced materials, medical tubes, custom SoCs/ASICs, imaging products, microcontrollers and wireless components that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's fifth largest semiconductor manufacturer (Gartner, 2012 Worldwide Semiconductor Revenue, April, 2013). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 210,000 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
OPTO 14 703