March 19, 2014
New Lineup Improves Power Efficiency, Reduces Product Footprint
FORT WORTH, Texas, — This week at APEC 2014, Toshiba America Electronic Components, Inc., (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, has introduced a new series of high-speed switching type super junction MOSFETs. The new DTMOS IV-H series consists of the TK31N60X, TK39N60X and TK62N60X, and is based on Toshiba's fourth generation 600V super junction MOSFET DTMOS IV series.
Using Toshiba's single epitaxial process, the new DTMOS IV-H series of super junction MOSFETs is suited to applications that require high reliability, power efficiency and a compact design, such as high efficiency switching power supplies for servers and telecom base stations; and as power conditioners for photovoltaic inverters. The new series achieves a high speed switching performance while keeping the low ON-resistance level of conventional DTMOS IV - all without loss of power. This is accomplished through the reduction of parasitic capacitance between Gate and Drain, which also contributes to improved power efficiency and downsizing of products.
According to Taka Ichikawa, business development manager for TAEC, "Superjunction DTMOS IV technology delivers many benefits to designers, helping them make resulting applications more efficient in terms of power and footprint."
The new DTMOS IV-H series will be highlighted in Toshiba's booth #613 on the APEC show floor in Fort Worth, Texas from March 16-20.
Part Number | Package | Absolute Maximum Rating | >RDS(ON) MAX (Ω) at VGS=10V |
Qg Typ. (nC) |
Ciss Typ. (pF) |
|
VDSS (V) |
ID (A) | |||||
TK31N60X | TO-247 | 600 |
30.8 | 0.088 | 65 | 3000 |
TK39N60X | TO-247 | 600 |
38.8 | 0.065 | 85 | 4100 |
TK62N60X | TO-247 | 600 | 61.8 | 0.040 | 135 | 6500 |
Additional package options, including 8x8mm DFN, TO-220 and TO-220SIS, are being added and will be available soon.
The new super junction MOSFETs are available now. Please contact your local Toshiba Sales Office for samples and pricing.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, December 2013). Toshiba Corporation was founded in 1875 and today has over 554 subsidiaries and affiliates, with 206,087 employees worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Toshiba America Electronic Components, Inc. All rights reserved. Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
POWR 14 706