July 23, 2014
ASIL D compliant IC targets electric power steering, features failure detection
SAN JOSE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the TB9052FNG motor pre-driver IC. The new device was developed for safety-critical automotive applications such as electric power steering (EPS) and other systems compliant with Automotive Safety Integrity Level D (ASIL D), the most rigorous measure defined within functional safety standard ISO 26262.
"As electrical systems within vehicles become increasingly sophisticated, there is a concurrent need for components that support and enable the most advanced safety features," said Deepak Mithani, senior director, Mixed Signal Business Unit at TAEC. "Toshiba is committed to helping the automotive industry implement new safety measures by continuing to develop motor drivers that support these requirements."
In addition to the main pre-driver circuit, TB9052FNG features a built-in motor current detection circuit in a redundant configuration, reducing board size and system complexity while contributing to functional safety. Also contributing to functional safety are the product's range of circuits that detect system failures, including battery under-voltage, 5V under voltage, over temperature and driver electrical short.
The TB9052FNG pre-driver IC has four channels, two high-side and two low-side, and includes a charge pump to solely drive N-channel MOSFETs. It is contained in a HTSSOP48-P-300-0.50 package measuring 12.5 x 6.1 x 1.2mm. Operating voltage range is +6 to 18V and operating temperature range is from -40 to +125 degrees C.
Sample shipments will start in August, with mass production scheduled to begin in March 2015. Toshiba will also be supplying associated safety analysis documentation.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.
APIC 14 715