September 17, 2014
New LEDs Simplify General Purpose and Industrial Lighting Designs
IRVINE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced that it has extended its LETERAS™1 family of white LEDs. The new TL1L3 series features ultra-compact devices that combine cost-effective gallium nitride-on-silicon (GaN-on-Si) chips with an industrial standard 3535 lens type package.
High-performance white LEDs are typically fabricated on expensive sapphire substrates using relatively small 100mm or 150mm wafers. Toshiba's LETERAS LEDs use a cost-effective GaN-on-Si process technology that allows GaN LEDs to be produced on 200mm silicon wafers, which lowers costs for manufacturers of general purpose and industrial LED lighting. The integrated lenses in Toshiba's newest LEDs make them suitable for implementation in security lighting, road lights, LED bulbs, down lights, and more. .
"White LEDs consume very little power and have long lives compared to incandescent light sources," stated Joseph Tso, business development manager for TAEC's optoelectronics group. "These two factors are major contributors to LEDs gaining widespread adoption in the general purpose lighting market, as well as a wide array of specialized lighting applications. LEDs are estimated to make up 53 percent of the global lighting market over the next few years, and the time is now to transition from standard lighting2. Our LETERAS family gives designers the flexibility to make this transition - no matter what the end application."
Devices in the TL1L3 series of 1.0W LEDs are housed in a 3.5mm x 3.5mm package, with a height (including the lens) of just 2.42mm. Despite their small size, the LEDs deliver up to 145 lumens (typ), depending on the correlated color temperature (CCT) .
The new TL1L3 LED series features seven devices that offer color temperatures from 2700K to 6500K. Minimum color rendering index (Ra) ratings of up to 80 contribute to natural-looking lighting. A low typical forward voltage (VF) of just 2.85V (at a forward current of 350mA) helps to keep power consumption at a minimum .
TL1L3 LEDs are rated for operating temperatures between -40°C and 100°C and have a maximum power dissipation of 3.4W. Additionally, they offer a very low typical thermal resistance Rth (j-s) from LED junction to solder point of only 5°C/W .
For more details, samples and pricing information, please contact your local Toshiba Sales Office.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
1LETERAS is a trademark of Toshiba Corporation
2Source: Statista.com.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.
OPTO 14 724