September 3, 2014
Feature Compact Packages; Optimized Diode Process for use in Small, Portable Consumer Devices
IRVINE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced two new series of 0.5 to 1.5A class Schottky Barrier Diodes (SBD): the S30 series (30V type) and S40 series (40V type). With options available in a compact 1.0x0.6 mm package size, the new SBDs are well-suited to smart phones and tablet PCs . They also function as highly efficient circuits for wireless power supplies.
Featuring twelve new devices, Toshiba's expanded lineup of SBDs now includes a high peak reverse voltage type (VRM=40V) and a high average rectifying current type (IO=1.5A). Additionally, the new CUS05S30 boasts low VF characteristics and reduces capacitance between terminals (Ct) by 50 percent or more when compared with current products1. All of the new devices achieve low VF characteristics by optimizing the diode process. This lower voltage drop provides higher switching speed and better system efficiency.
Additionally, four other package types are available, ranging from the small SOD-882 (CST2: 1.0x0.6mm) to the standard SOD-323 (USC: 2.50x1.25mm) ? making Toshiba's SBDs suitable for a number of different applications with varying mounting size requirements.
Absolute Maximum Ratings | Package | ||||
---|---|---|---|---|---|
IO | VRM | CST2 (1.0x0.6mm) |
CST2B (1.2x0.8mm) |
CST2C (1.6x0.8mm) |
USC (2.5x1.25mm) |
0.5A | 30V | CTS05S30 | - | - | CUS05S30 |
40V | CTS05S40 | - | CUS05S40 | ||
1.0A | 30V | - | CBS10S30 | - | CUS10S30 |
40V | - | CBS10S40 | - | CUS10S40 | |
1.5A | 30V | - | - | CCS15S30 | CUS15S30 |
40V | - | - | CCS15S40 | CUS15S40 |
Toshiba's new Schottky Barrier Diodes are available now. Budgetary pricing is $0.022-$0.042. Please contact your local Toshiba Sales Office for samples and pricing.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
1i.e. Toshiba's CUS10xx, CUS15xx, CTS520, CTS521, and CBS05F30
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.
POWR 14 721