require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
November 19, 2014
Protects High-Speed Interfaces from Static Electricity
IRVINE, Calif., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the introduction of a new ESD (electrostatic discharge) protection diode - the DF5G7M2N. Built to protect equipment attached to communication lines, the DF5G7M2N shields high-speed interfaces such as USB3.1, HDMI®, DisplayPortTM and Thunderbolt™ from static electricity. It can also be used to protect small portable devices such as smartphones and tablets from ESD events.
Housed in a DFN5 package that reduces its footprint to less than 50 percent of that of similar products1, the DF5G7M2N simplifies wiring design, making it suitable for high density mounting. Additionally, Toshiba's new ESD diode realizes low capacitance and low dynamic resistance by optimizing the process, suppressing signal quality deterioration and providing high ESD resistance.
"Static electricity on high speed data lines can cause numerous problems, including effecting quality and reliability," noted Talayeh Saderi, senior business development manager for TAEC. "Our new ESD diode helps to provide stable operation and reliability for these voltage-sensitive lines."
Part number | VRWM max(V) | VBR min @ IBR =1mA (V) | IR max @ VRWM =5.5 V (µA) |
CT typ. @ VR =0V, f=1Mhz (pF) | RDYN typ. @ TLP evaluation (Ω) | Package | |||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
DF5G7M2N | 5.5 | 6.0 | 0.05 | 0.2 | 1 | DFN5 |
Toshiba's new ESD diode is available now, with budgetary pricing estimated at $0.06. Please contact your local Toshiba Sales Office for samples.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
1Comparison with DF10G7M1N (DFN10: 2.5x1.0 mm, 4bit)
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.
HDMI® is a registered trademark of HDMI Licensing, LLC in the U.S. and other jurisdictions
DisplayPort™ is a trademark of Video Electronics Standards Association in the United States and/or other countries
Thunderbolt™ is a trademark of Intel Corporation in the United States and/or other countries
LGSS 14 731