January 14, 2015
VSON4 Packages Reduce Mounting Area by 50 Percent
IRVINE, Calf., — Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the expansion of its lineup of ultra-small photorelays with the addition of four products: the TLP3417, TLP3420, TLP3440 and TLP3475. The new products are suited for system solutions in various applications, including semiconductor testers, measurement equipment, probe cards and medical equipment.
The new products are housed in the industry's smallest package1 for photorelays, the Toshiba-developed VSON42 package. The VSON4 package enables high-density assembly and, by replacing USOP4 packages, can shrink the assembly area by 50 percent and the assembly volume by 60 percent.
The TLP3440 has improved leakage characteristics against high frequency at off-state, while the TLP3475 has improved high speed signal transmission characteristics at on-state3. For high voltage measurement requirements, including SoC testing, the TLP3417 supports 80V, while the TLP3420 supports 100V. The new products have the same electrical characteristics as the conventional Toshiba USOP4 series products, making it easier to evaluate them as replacement products. All devices achieve 3mA (max) trigger LED currents and 300Vrms (min) isolation voltages.
Key Specifications of the New Products | ||||
---|---|---|---|---|
Features | Features | For High Voltage Systems | ||
Product | TLP3440 | TLP3475 | TLP3417 | TLP3420 |
Package | VSON4 Package Area: 1.5mm (max.) x 2.5mm (max.), Height: 1.3mm (max.) |
|||
On-state Current | 0.12A (max.) | 0.3A (max.) | 0.12A (max.) | 0.08A (max.) |
On-state Resistance | 12Ω (typ.) | 1Ω (typ.) | 7Ω (typ.) | 8Ω (typ.) |
Off-state Voltage | 40V (min.) | 50V (min.) | 80V (min.) | 100V (min.) |
Off-state Capacitance (Photo Side) |
0.45pF (typ.) | 12pF (typ.) | 5pF (typ.) | 6pF (typ.) |
Trigger LED Current | 3mA (max.) | |||
Isolation Voltage | 300Vrms (min.) |
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today's leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's sixth largest semiconductor manufacturer (Gartner, 2013 Worldwide Semiconductor Revenue, April 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
For additional company and product information, please visit http://www.toshiba.com/taec/.
1For photocoupler products, as of September 8, 2014. Toshiba survey.
2VSON: Very Small Outline Non-leaded.
3When compared to previous Toshiba products.