August 11, 2015
Features Industry-Leading Low Drop-Out Characteristics at Low Voltage Input
IRVINE, Calif., -- Toshiba America Electronic Components, Inc. (TAEC)*, a committed leader that collaborates with technology companies to create breakthrough designs, today announced the launch of the TCR5AM series, a new lineup of 500 mA output low-drop out (LDO) regulator integrated circuits (IC)s. These single-output voltage regulators are available in fixed output voltages between 0.55 V and 3.6 V and are capable of driving up to 500 mA. The TCR5AM series is suited to WIFI chipsets, cameras, power management applications for smart phones, tablets, and wearables - and any application requiring an LDO where battery power is critical.
Toshiba has achieved industry-leading1 LDO characteristics for the new series by adopting an external bias voltage terminal (VBAT) that is separated from the power source input. This sets the new voltage regulators apart from conventional products and enables them to increase the efficiency of the power source. Additionally, the TCR5AM series incorporates protection functions such as over-current protection and over-temperature protection, making them a safe, efficient LDO solution.
TCR5AM series |
|||||||
---|---|---|---|---|---|---|---|
Part number |
Output voltage typ. (V) |
Part number |
Output voltage typ. (V) |
Part number |
Output voltage typ. (V) |
Part number |
Output voltage typ. (V) |
TCR5AM055 |
0.55 |
TCR5AM11 |
1.1 |
TCR5AM20* |
2.0 |
TCR5AM295* |
2.95 |
TCR5AM06 |
0.6 |
TCR5AM115* |
1.15 |
TCR5AM21* |
2.1 |
TCR5AM30 |
3.0 |
TCR5AM065* |
0.65 |
TCR5AM12 |
1.2 |
TCR5AM22* |
2.2 |
TCR5AM31 |
3.1 |
TCR5AM07* |
0.7 |
TCR5AM125* |
1.25 |
TCR5AM23* |
2.3 |
TCR5AM32* |
3.2 |
TCR5AM075* |
0.75 |
TCR5AM13* |
1.3 |
TCR5AM24* |
2.4 |
TCR5AM33 |
3.3 |
TCR5AM08* |
0.8 |
TCR5AM14* |
1.4 |
TCR5AM25 |
2.5 |
TCR5AM34* |
3.4 |
TCR5AM085* |
0.85 |
TCR5AM15 |
1.5 |
TCR5AM26* |
2.6 |
TCR5AM35* |
3.5 |
TCR5AM09* |
0.9 |
TCR5AM16* |
1.6 |
TCR5AM27* |
2.7 |
TCR5AM36 |
3.6 |
TCR5AM095* |
0.95 |
TCR5AM17* |
1.7 |
TCR5AM28 |
2.8 |
|
|
TCR5AM10 |
1.0 |
TCR5AM18 |
1.8 |
TCR5AM285* |
2.85 |
|
|
TCR5AM105 |
1.05 |
TCR5AM19* |
1.9 |
TCR5AM29 |
2.9 |
|
|
Toshiba's new output LDO regulator ICs are available now. Please contact your local Toshiba Sales Office for samples.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor manufacturer and the world’s sixth largest semiconductor manufacturer (Gartner, 2014 Worldwide Semiconductor Revenue Estimates, December 2014). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
*For information on products marked with *, please contact our sales division.
1In the category of 500 mA LDO regulator ICs in a package under 1 mm square, as of February 16, 2015. Toshiba survey.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.