Toshiba Launches Industry’s Smallest 1.3A LDO Regulator

April 12, 2017

Targeted to Mobile Power Applications; Featuring Space Savings, Low Power Consumption, High Ripple Rejection Ratio

Toshiba TCR13AGADJ Regulator

IRVINE, Calif., --- Toshiba America Electronic Components, Inc. (TAEC)* today announced the introduction of the industry’s smallest1 1.3A output current CMOS low dropout (LDO) regulator: the TCR13AGADJ. Housed in a WCSP6F package, the TCR13AGADJ measures just 0.8mm x 1.2mm, with a maximum thickness of 0.33mm. These dimensions make it suitable for space-conscious applications. 

The TCR13AGADJ has an industry-leading1 high typical ripple rejection ratio (90dB  @Vout=0.9V, f=1kHz) which helps significantly reduce ripple noise from DC-DC converters and PMIC. Ripple noise is a common problem encountered by designers when attempting to supply power to camera and RF parts.

Toshiba’s new LDO regulator can be used in a variety of applications that require stable output voltage at high output currents with low power consumption. These include Wi-Fi® chipsets for smartphones and tablets, as well as power supplies for cameras and RF modules. It can also be used in power supply control for wearable devices, notebook PCs, digital video cameras, storage products, and set-top boxes. By using an external bias power supply terminal (VBAT), the new regulator achieves a leading-class1 low typical dropout voltage of 92mV (@Vout=0.9V,  Iout=1.0A). Maximum dropout voltage is rated at 163mV (@Vout=0.9V, Iout=1.0A).

The WCSP6F package is the industry’s smallest package for 1.3A LDO regulators, enabling it to be used in mobile and module applications that require small footprints and low profiles. Using an external resistor, the output voltage of the TCR13AGADJ can be adjusted over a wide range of 0.55V to 3.6V. Integrated capabilities include over-current protection, over-temperature protection, inrush current protection, and an auto discharge function.

Additional Features

  • Fast load transient response -100/+115mV (typ.) @0.01A⇔1A, COUT>4.7μF
  • Under-voltage-lockout function
  • Soft start function
  • Pull down connection between CONTROL and GND
  • Stable with over 4.7μF input capacitor, 1.0μF bias capacitor and 4.7μF output ceramic capacitor

Pricing and Availability

Toshiba’s new regulator is available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide (as of March 31, 2016). Visit Toshiba's web site at http://toshiba.semicon-storage.com.

1In the category of 1.3A output current LDO regulators, as of December 5, 2016. Toshiba survey.
* Wi-Fi is a registered trademark of Wi-Fi Alliance.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

A new window will open