require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
June 25, 2018
Toshiba’s MG07 14TB SATA HDD completed qualification on Select Supermicro Storage Server platforms
Irvine, Calif. — Toshiba America Electronic Components, Inc. (“TAEC”) today announced that Super Micro Computer, Inc. has successfully qualified the MG07ACA Series 14TB1 and 12TB HDD SATA models on select Supermicro storage server platforms. Using a 9-disk, helium-sealed design, the new MG07ACA Series provides power-efficient capacity and storage density, which is now available on Supermicro’s popular SuperStorage (SSG) line-up of server platforms. The MG07 Series industry-leading 14TB capacity allows data center customers a choice of storage server platform solutions available through Supermicro’s extensive network of distributors as well as systems and solutions integrators.
“As we continue to develop solutions to meet the growing capacity needs of enterprise and cloud data center customers, Toshiba is pleased to be working with Supermicro on solutions utilizing our new MG07ACA Series helium-sealed HDD,” said Kyle Yamamoto, Vice President of HDD Business Unit, Toshiba America Electronic Components, Inc. “Toshiba’s innovative, power-efficient 9-disk design delivers the highest capacity available in the market today using conventional magnetic recording, and matches up well with Supermicro’s highly-regarded lineup of server and storage solutions.”
“Being first-to-market with storage servers qualified to support 14TB hard drives puts Supermicro and Toshiba in a strong position to better support our customers with high-capacity storage solutions,” said Michael McNerney, vice president, Software Solutions and Network Security, Supermicro. “Leveraging Supermicro’s complete portfolio of open industry standard storage optimized servers with maximum efficiency, customers can now maximize the storage capacity per server node by using 14TB SATA drives and achieve even better cost per TB.”
The MG07ACA Series features both 14TB 9-disk and 12TB 8-disk models. The helium-sealed 3.5-inch2 mechanical design realizes better storage density and a lower HDD operating power profile, achieving a 40% increase in maximum capacity and 50% better power efficiency (W/GB) over 10TB HDD models.
The 14TB and 12TB MG07ACA Series SATA disk drives are available to order today as disk options for select SuperStorage (SSG) server models from Supermicro.
For more information on the MG07ACA Series visit https://toshiba.semicon-storage.com/us/product/storage-products/enterprise-hdd/mg07acaxxx.html. To view Toshiba’s full line of HDD storage products, please visit: https://toshiba.semicon-storage.com. To learn more about our storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and follow @ToshibaStorage on Twitter.
To learn more about Supermicro storage server products and solutions, please visit http://www.supermicro.com/products/nfo/storage.cfm.
Toshiba America Electronic Components Inc. is an independent operating company owned by Toshiba America, Inc., and is the US based electronic components business of Toshiba Electronic Devices and Storage Corporation in Japan. TAEC offers consumers and businesses a wide variety of innovative hard disk drive (HDD) products plus semiconductor solutions for automotive, industrial, IoT, motion control, telecoms, networking, consumer and white goods applications. The company’s broad portfolio encompasses integrated wireless ICs, power semiconductors, microcontrollers, optical semiconductors, ASICs, ASSPs and discrete devices ranging from diodes to logic ICs. For more company information visit TAEC’s web site at www.toshiba.com/taec.
1Definition of capacity: A terabyte (TB) is 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1TB = 240= 1,099,511,627,776 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
2Form Factor: "3.5-inch" means the form factor of HDDs. They do not indicate drive's physical size
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Company names, product names, and service names mentioned herein may be trademarks of their respective companies.