require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
February 7, 2020
TOKYO — Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched “TC78H670FTG,” the latest addition to its line-up of micro-stepping motor driver ICs. The new IC has a maximum rating of 18V/2.0A[1] and can drive motors with a wide range of operating voltages. Mass production starts today.
The new IC can drive a 128 micro-stepping motor with a power supply ranging from 2.5V to 16V. Its wide range of applications includes USB-powered, battery-powered, and standard 9-12V system devices, and it can also be used with a 1.8V interface, allowing connection to various hosts and microcontrollers.
Toshiba’s newest[2] DMOS process ensures that TC78H670FTG realizes excellent figure-of-merit low ON resistance. The process also contributes to the IC’s ultra-low standby current. The IC is housed in a compact QFN16 package and eliminates use of a current sense resistor by incorporating a current detection part that contributes to lower cost, a smaller component footprint, and PCB routing space savings.
Cameras, security cameras, portable printers, handheld scanners, pico-projectors, and smartphones
Note:
[1] Actual motor drive current depends on the use environment and such factors as ambient temperature and power supply voltage.
[2] As of February 2020.
[3] Compared to the existing products manufactured by Toshiba.
For more information about the new product, please visit:
To check availability of the new product at online distributors, please visit:
*Company names, product names, and service names may be trademarks of their respective companies.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.