Contact us

Uma nova janela será aberta Uma nova janela será aberta

Are decoupling capacitors required across power and ground lines?

Decoupling capacitors are required in order to stabilize IC operation by reducing the impedance of power lines and to absorb back-EMF from the motor coil when it is de-energized.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.