Contact us

Uma nova janela será aberta Uma nova janela será aberta

Do linear-type local power supply ICs (linear regulators) need external parts?

External parts are not needed as shown in the figure below. (Input and output capacitors are needed.) Output voltage becomes constant by operating a MOSFET as a variable resistor so that VOUT is constant.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.