Contact us

Uma nova janela será aberta Uma nova janela será aberta

How can I prevent the output voltage from overshooting following the application of the control voltage to an LDO?

To prevent the output voltage from overshooting, use an LDO with a soft-start or inrush current limiting function. The soft-start function raises the output voltage slowly after the control voltage is applied to an LDO.

To perform a parametric search of LDOs with a soft-start or inrush current limiting function, click:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.