Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the meaning of “Logic-Level Gate Drive” for the MOSFET?

It means the MOSFET can be driven by the output voltage (4 to 5 V) of general-purpose logic IC.
When the general-purpose logic IC does not have enough output current capability, the MOSFET cannot be driven.
In such a case, consider changing the drive circuit.

For MOSFET’s drive, please refer to “MOSFET Gate Drive Circuit:Power MOSFET Application Notes.”

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.