Contact us

Uma nova janela será aberta Uma nova janela será aberta

How much resistance variation do BRTs exhibit?

±30% relative to the typical resistance.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.