Contact us

Uma nova janela será aberta Uma nova janela será aberta

Is it OK to use the internal resistors of a BRT as separate resistors instead of as bias resistors for a transistor?

It is possible, but it is recommended to use discrete resistors, considering the resistance variation, power dissipation, operating voltage range and temperature characteristics.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.