Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is the relation between base-emitter current and collector-emitter current in a bipolar transistor?

When small current (IB) flows from base to emitter, current of IB x hFE flows from collector to emitter in NPN transistor.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.