Contact us

Uma nova janela será aberta Uma nova janela será aberta

I heard that a junction FET could be used as a constant-current source. How can I create a constant-current source?

When a junction FET is connected as shown below, it acts as a pseudo-constant-current diode.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.