Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is a MOSFET?

MOSFET stands for metal-oxide-semiconductor field-effect transistor. It is a field-effect transistor with a MOS structure. Typically, the MOSFET is a three-terminal device with gate (G), drain (D) and source (S) terminals. Current conduction between drain (D) and source (S) is controlled by a voltage applied to the gate (G) terminal. MOSFETs compare favorably with bipolar transistors in terms of relatively high-speed and low-loss operation. There are P type and N type by channel polarity, and there are enhancement type with normally off (gate voltage 0 V off) and depletion type with normally on (deactivated with gate voltage 0 V) by control method. Enhancement type is popular.

For an explanation of the MOSFET structure, please refer to the following document.
Structures and Characteristics: Power MOSFET Application Notes (PDF:484KB)
https://toshiba.semicon-storage.com/info/docget.jsp?did=13413

Example of an N-Channel MOSFET

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.