Contact us

Uma nova janela será aberta Uma nova janela será aberta

Are there any special considerations for using IGBTs?

As is the case with a MOSFET, the gate (G) input of an IGBT has high impedance. It is recommended to drive the gate input with a low-impedance driver so that it will not be affected by noise.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.