Contact us

Uma nova janela será aberta Uma nova janela será aberta

LED Drivers

Toshiba offers a broad array of LED drivers featuring constant-current drivers with excellent LED current accuracy. Included in the Toshiba LED driver portfolio are not only standard LED drivers, but also those with PWM dimming control, current gain control and various error detection functions. Toshiba product lineup also includes LED drivers with a DC-DC converter making them suited for mobile equipment applications.

LED Drivers by Application

Click the following links to find information about Toshiba LED drivers designed specifically for each application.

Cross Reference Search

  • Cross-reference search is a search service which offers you suitable Toshiba products from other manufacturers' products.

Frequently Asked Questions

  • Frequently Asked Questions are here.

Downloading PSpice® models

pspice-img
Downloading PSpice® models
[Download Flow]
  1. Click on the 'Go to the Agreement page' button below and read the terms of use for the PSpice® models. If you accept all the terms, select the 'Yes' radio button and click the button 'I understand and agree'.
  2. This will take you to the online registration form. Fill in the form. Confirm that all the data are correct, and click the 'Send' button.
  3. You will receive an on-screen confirmation message acknowledging that your registration has been accepted. You will thereafter receive download information at your registered email address.
  4. Click on the URL embedded in the email and download the desired PSpice® models.

    PSpice® models are provided as zip-compressed files.
    To run a simulation, you need to prepare a PSpice® simulation environment.
    PSpice is a registered trademark of Cadence Design Systems, Inc.

Go to the Agreement page.

LED Drivers with PSpice models list

Introduction of an Evaluation Board

Vendor Name Product Name Outline
MARUTSU ELEC CO.,LTD.
(Japanese language only)
TC62D902FG A photo of evaluation board for an LED power control IC for lighting applications.
  • Evaluation board for an LED power control IC for lighting applications
    This evaluation board incorporates the TC62D902FG for LED power control designed for the isolated flyback topology. The TC62D902FG controls the average LED current via the peak current level of the primary side of a transformer and the control pulse width, eliminating the need for an LED current detection circuit on the secondary side.

    This evaluation board operates from a 100-VAC power supply. You can experiment with TRIAC-dimming LED lighting applications just by attaching an LED load with a 13- to 24-V output and a TRIAC dimmer to the board.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.