Contact us

Uma nova janela será aberta Uma nova janela será aberta

NAND Flash Memory with an Integrated Controller

Related Information

Memory Microsite | Memory Blog

NAND Flash Memory Solutions with Integrated Controller chip in a Package

If you opt for raw NAND(NAND Flash Memory) chips, ECC(Error Correction Code), bad-block management, logical-to-physical address conversion, wear leveling (a technique for distributing re-writes evenly across a memory array) and other control functions must be implemented on the host side. With evolving NAND manufacturing processes, ECC is becoming notably more sophisticated, imposing heavier burdens on the host processor, especially for large-capacity NAND.

In response to customer needs, Toshiba offers NAND Flash Memories that integrate a controller in the same package. These are Toshiba’s recommendation for  high-capacity NAND Flash Memories.

Features of NAND Flash Memories with an Integrated Controller

Toshiba offers e-MMC and UFS, a family of high-capacity NAND Flash Memories that integrates a controller in one package. These NAND

solutions provide ECC and other control functions, optimized by Toshiba for each NAND technology generation.

e-MMC and UFS reduce the workload on the host processor, simplify product development, shorten time-to-market and increase ease of use of memory products.

nand_lineup

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.