3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
October 19, 2020
Toshiba Electronic Devices & Storage Corporation
TOKYO— Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has launched “TW070J120B,” a 1200V silicon carbide (SiC) MOSFET for industrial applications that include large capacity power supply. Shipments start today.
The power MOSFET using the SiC, a new material, achieves high voltage resistance, high-speed switching, and low On-resistance compared to conventional silicon (Si) MOSFET, IGBT products. Therefore, it will contribute to lower power consumption and system downsizing.
Fabricated with Toshiba’s second-generation chip design[1], which improves the reliability of SiC MOSFET, the new device realizes low input capacitance, a low gate-input charge, and low drain-to-source On-resistance. Compared with “GT40QR21,” Toshiba’s 1200V silicon insulated gate bipolar transistor (IGBT), it cuts turn-off switching loss by about 80% and switching time (fall time) by about 70%, while delivering low On-voltage characteristics with a drain current of 20A or less[2].
Gate threshold voltage is set in the high range of 4.2V to 5.8V, which reduces malfunction risk (unintended turn on or off). Incorporation of an SiC Schottky barrier diode (SBD) with low forward voltage also helps to reduce power loss.
The new MOSFET will contribute to higher efficiency by reducing power loss in industrial applications, such large capacity AC-DC converters, photovoltaic inverter, and large capacity bidirectional DC-DC converters, and will also contribute to reduced equipment size.
Notes:
[1] Toshiba’s news release on July 30, 2020: “Toshiba’s New Device Structure Improves SiC MOSFET Reliability”
[2] ambient temperature 25°C
(Unless otherwise specified, Ta=25℃)
Part number |
Package |
Absolute maximum ratings |
Electrical Characteristics |
Sample Check & Availability |
|||||
---|---|---|---|---|---|---|---|---|---|
Drain- source voltage VDSS (V) |
Drain current (DC) ID @Tc=25℃ (A) |
Drain- source On-resistance RDS(ON) typ. @VGS=20V (mΩ) |
Gate threshold voltage Vth @VDS=10V, ID=20mA (V) |
Total gate charge Qg typ. (nC) |
Input capacitance Ciss typ. (pF) |
Diode forward voltage VDSF typ. @IDR=10A, VGS=-5V (V) |
|||
TO-3P(N) |
1200 |
36.0 |
70 |
4.2 to 5.8 |
67 |
1680 |
-1.35 |
Follow the link below for more on the new product.
Follow the link below for more on Toshiba SiC MOSFETs.
Follow the link below for more on Toshiba SiC Power Devices.
*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.