Contact us

Uma nova janela será aberta Uma nova janela será aberta

How can I calculate the junction temperature of an LDO?

The maximum junction temperature of an LDO can be calculated from its power consumption and thermal resistance using Equations 1 and 2.

Absolute maximum rated junction temperature specified

For example, suppose that VIN=1.5 V, VOUT=1 V, IOUT=200 mA, IB=20 μA, PD=0.6 W, and Ta=60°C. Then, the maximum junction temperature of the LDO can be calculated as follows.

From Equation 1, power consumption (P) is calculated as follows:

Power consumption

From Equation 2, the maximum junction temperature is calculated as follows:

Absolute maximum rated junction temperature specified

Circuit diagram

Allow a sufficient temperature margin for the thermal design of an LDO application.

Also see the following documents and web page for a description of junction temperature:
For other LDO regulators, visit the main web page of LDO regulators at:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.