Contact us

Uma nova janela será aberta Uma nova janela será aberta

Hands-free

Automotive information products and mobile devices offer high performance and are popular in today's market. This equipment provides important information and comfort to the driver, yet to ensure safety certain restrictions must be followed.

The Toshiba Bluetooth® LSI for car audio and navigation can provide higher connectivity with cellular phones. In addition, the high-performance on-chip processor in the Bluetooth LSI with various middleware provides a comfortable hands-free system and supports a wireless audio streaming function.

Bluetooth Hands-Free Systems

Bluetooth Front-End Solutions

A hands-free Bluetooth system can be created by connecting an external DSP to the TC35661 Bluetooth IC. The integrated ARM® ARM7™ processor provides control over Bluetooth pairing with a mobile phone, and sends and receives voice signals for telephone calls.
The ARM7™ processor passes voice data to/from the external DSP via an I2S interface, which, in turn, provides echo cancellation (EC) and noise reduction (NR) to enable hands-free, in-vehicle telephone calls.

This is the system block diagram of using the TC35661.

* ARM is a registered trademark of ARM Limited in the EU and countries elsewhere. ARM7 is a registered trademark of ARM Limited (or its subsidiary) in the EU and countries elsewhere.

* Bluetooth is a registered trademark owned by Bluetooth SIG, Inc. and any use of such marks by Toshiba is under license.

* System and product names mentioned herein may be trademarks or registered trademarks of respective companies or organizations.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.