Contact us

Uma nova janela será aberta Uma nova janela será aberta

How many watts does the REXT resistor need to be rated at?

The REXT pin is a constant-voltage output. The output voltage is somewhere around 1 V, but it differs slightly from device to device. The permissible power of the resistor can be calculated as V2/REXT. 1/8 or 1/16 W will do.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.