Contact us

Uma nova janela será aberta Uma nova janela será aberta

A junction FET is widely used for impedance conversion. What is it for?

Generally, the gate input terminal (G) of an FET has high impedance. A typical application of a junction FET is a source follower circuit where an output load resistor is connected to the source (S) terminal as shown below. Its gain is approximately 1.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.