Contact us

Uma nova janela será aberta Uma nova janela será aberta

What is a JFET?

JFET stands for junction-gate field-effect transistor. Formerly, when one simply said "FET," one meant a JFET. Key features of JFETs include a large input impedance and low noise, making them suitable for impedance conversion and low-noise amplifier applications.
A JFET can also be used as a simple constant-current source.

Example of an N-Channel JFET

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.