Contact us

Uma nova janela será aberta Uma nova janela será aberta

List some application examples for IGBTs.

Because of the high-voltage and high-current features, medium- to large-sized IGBTs are widely used for applications in which a large current continuously flows, such as uninterruptible power supply (UPS), motor drive circuits and induction cooktops.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.