Contact us

Uma nova janela será aberta Uma nova janela será aberta

What are RC-IGBTs?

The structure of an RC-IGBT is shown in the figure below. A diode is made by forming N layer partially in P layer that works as a collector of the IGBT. This diode works as a Free Wheeling Diode (FWD) that is generally inserted in a circuit with an IGBT.

Structure of RC-IGBT

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.