Contact us

Uma nova janela será aberta Uma nova janela será aberta

High-precision overvoltage clamp function

The overvoltage clamp function limits the output voltage to the limit voltage when the limit voltage is exceeded. Toshiba eFuse IC has a function to prevent excessive voltage from being applied to the ICs at subsequent stages by clamping the output voltage to the specified output voltage of individual products.

High-precision overvoltage clamp function

Our eFuse IC has an overvoltage clamping function. For example, in the case of the TCK805, even if the input voltage increases, the input voltage is suppressed to the about 6.0-V (typ.). Therefore, even if the input voltage instantaneously becomes excessive, more stable power supply can be provided by keeping the output voltage with this clamp function and keeping it within the withstand voltage of the post-stage IC.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.