Contact us

Uma nova janela será aberta Uma nova janela será aberta

High-resolution PPG Output

Moving distance and speed of a rotor of an ultrasonic motor are controlled by frequency, amplitude and a time interval of the ultrasonic wave. Toshiba has produced TX03 series microcontrollers incorporating high-resolution PPG outputs. The microcontrollers achieve quite fine control in the moving distances of rotors.

ppg_e

Operating Principle of Ultrasonic Motor

An ultrasonic motor is driven by ultrasonic waves of which frequency is more than 20kHz. A rotor is moving on a stator which transfers the ultrasonic waves. Piezoelectric devices generate up-and-down movement when AC voltage is applied to. The stator transfers the movement from the bottom to the surface. A traveling-wave to the right on the stator pushes the rotor toward opposite direction, that is, to the left. Because the up-and-down swings at the stator surface make counterclockwise rotation, which results in the rotor’s movement to the left.

ppg01_e

Product List

TX03 series products incorporating a High-resolution PPG output are displayed.

Contatos

Se você tiver alguma dúvida, clique em um destes links:

Dúvidas técnicas
Dúvidas sobre compras, exemplos e confiabilidade de IC
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.