News Center

This page is listing links of the press release and topics published by Toshiba Electronic Devices and Storage Corporation.
Information in the news and topics, including product prices and specifications, content of services and contact information, is current on the date of the news announcement, but is subject to change without prior notice. The news before March 31, 2017 is the news published by Toshiba Storage & Electronic Devices Solutions Company.

Release Year
Category
News Category
15-05-2024
Expanded Lineup of Surge Protection Zener Diodes that Support the Quality Improvement of Electronic Equipment by Adding New Voltage Ranks
22-11-2023
東芝適用於高壓電路的400 V耐壓小型開關二極體
30-08-2023
東芝推出20款適用於汽車設備的突波保護齊納二極體產品
25-07-2022
過壓保護齊納二極體採用超小型SOD-962封裝,有助於設備上高密度打件
30-06-2022
採用壓裝式封裝的快速恢復二極體有助於減小電源轉換器的尺寸和功耗
17-06-2022
新增的SOT-23封裝浪湧保護齊納二極體產品線擴展有助於電子設備品質改善
24-02-2022
東芝推出超低電容TVS二極體,可保護物聯網設備高頻天線免受ESD侵擾
18-02-2022
東芝電源電路保護用齊納二極體產品線擴展,有助於提升產品的可靠性
22-01-2021
Lineup expansion of Schottky barrier diodes with 60 V products using the compact US2H package that has excellent heat dissipation allowing easier thermal design : CUHS15F60, CUHS20F60, CUHS15S60, CUHS20S60
18-08-2020
東芝推出可提高設備的可靠性的齊納二極體其適用於電源線浪湧保護
16-07-2020
Lineup expansion of SiC SBDs of 650 V contributing to high efficiency of power supply PFCs : TRS12N65FB, TRS16N65FB, TRS20N65FB, TRS24N65FB
26-05-2020
SiC SBDs of 650 V/12 A contributing to power saving and high efficiency of power supply PFCs : TRS12A65F, TRS12E65F
22-05-2020
Bidirectional TVS diode with a higher peak pulse current rating that contributes to improving reliability of the IC's power supply lines : DF2B5PCT, DF2B7PCT
17-10-2019
東芝推出適用於ThunderboltTM 3及其他高速訊號線的低電容TVS Diode
03-09-2019
Low capacitance TVS diodes for automotive applications offering fine protection performance while keeping signal quality at several Gbps : DF2S5M4FS, DF2S6M4FS
20-08-2019
A lineup expansion of TVS diodes for mobile devices by a product with an increased peak pulse current rating for improved surge protection performance: DF2B7BSL
10-07-2019
Toshiba expands lineup of SBD, which uses a compact package with high heat dissipation ability that allows easier thermal design, by 30 V/ 40 V products: CUHS20F40, CUHS20F30, CUHS15F40, CUHS15F30, CUHS20S40, CUHS20S30, CUHS15S40, CUHS15S30
28-03-2019
Expanded the lineup of general rectifier diodes that can reduce power consumption of equipment: CRG04A
19-12-2018
A TVS diode with an increased peak pulse current rating to improve surge protection performance for mobile devices: DF2B5BSL
13-12-2018
Consumption energy saving general-purpose rectifiers with high ESD protection ability: CRG09A, CRG10A
開啟新視窗