News Center

This page is listing links of the press release and topics published by Toshiba Electronic Devices and Storage Corporation.
Information in the news and topics, including product prices and specifications, content of services and contact information, is current on the date of the news announcement, but is subject to change without prior notice. The news before March 31, 2017 is the news published by Toshiba Storage & Electronic Devices Solutions Company.

Release Year
Category
News Category
05-06-2024
有助於實現工業設備高效化和小型化的1200V SiC MOSFET模組產品線擴展
03-06-2024
Toshiba Succeeds in Reducing On-resistance in SBD embedded SiC MOSFET While Securing Reliability and Short-Circuit Ruggedness
17-04-2024
擴大 U-MOSX-H 系列 150 V N 通道 MOSFET 的產品陣容,以降低電源功耗
06-03-2024
1700V SiC MOSFET模組的產品陣容擴大,有助於工業設備的高效化和小型化
22-02-2024
Toshiba推出有助於提高電源效率的帶高速二極體的功率MOSFET
06-12-2023
東芝擴展3300V SiC MOSFET模組的產品陣容,有助於工業設備的高效率化及小型化
07-11-2023
Toshiba推出適用於USB裝置和電池組保護的30V N溝道共漏MOSFET
20-09-2023
擴大有助於降低車載應用功耗的 40V N-Channel MOSFET 產品陣容
23-08-2023
東芝擴展U-MOSX-H系列80V N通道功率MOSFET產品線,協助降低電源功耗
17-08-2023
Toshiba推出採用新型封裝的車用40V N通路功率MOSFET,有助於汽車設備實現高散熱和小型化
29-06-2023
Toshiba推出支援電源電路小型化的100V N溝道功率MOSFET
28-06-2023
採用L-TOGL™封裝,支持大電流和高散熱的80V / 100V車載N溝道功率MOSFET的產品線擴展
14-06-2023
有助於降低車載設備功耗的-60V P通道功率MOSFET的產品線擴展
13-06-2023
Toshiba發布有助於提高電源效率的600V超接合結構N溝道功率MOSFET
18-05-2023
東芝推出小巧輕薄型共汲極 MOSFET,導通電阻極低,適合快速充電設備
30-03-2023
東芝發布150V N溝道功率MOSFET,具有業界領先的[1]低導通電阻和改進的反向恢復特性,有助於提高電源效率
15-02-2023
東芝採用新世代製程擴展150V N通道MOSFET產品線 - 藉此提高電源供應器的效率
31-01-2023
東芝推出採用新型高散熱封裝的車載40V N溝道功率MOSFET,支援車載設備對更大電流的需求
31-03-2022
東芝推出採用最新一代工藝的150V N通道功率MOSFET,可大幅提高電源效率
30-03-2022
用於車載設備的小型MOSFET產品線中新增了40 V產品,其低導通電阻有助於降低功耗
開啟新視窗