This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
When the output is turned on, the charging current flows through the output capacitor. If this current is too large, the overcurrent protection circuit may malfunction, making it impossible to start up, or the output voltage may overshoot. This function restricts the current flowing through the output capacitor to prevent this. Toshiba eFuse IC can reduce the inrush current by using an adjustable slew rate control function with an external capacitance.
The larger the output capacitor and the higher the input voltage, the higher the inrush current. This large inrush current may cause failure. In that case, it is effective to keep the inrush current low by the slew rate control function.Our eFuse IC can adjust the slew rate of the output voltage with a small external capacitance, which simplifies the design of circuits that suppress the inrush current.
Stock Check & Purchase
require 3 characters or more.
Part Number | Authorized Distributor | Stock Quantity | Date | Shopping Cart |
---|