Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is the voltage range in which IC couplers can operate?

The operating range of IC couplers is within the specified values for the power supply voltage VCC and the output voltage VO each. If any specified upper limit value is exceeded, the product may become severely damaged. If any specified lower limit value fails to be reached, a voltage allowing the circuit incorporated in the photodetector IC to operate correctly will not be distributed, and the product will become inoperable.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.