Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is a variable-capacitance diode?

Variable-capacitance diodes are abbreviated as VCDs. They are also called varicap diodes.
Variable-capacitance diodes has a variable capacitance which is a function of the voltage between anode and cathode.
General-purpose diodes are used for rectification and signal detection, and variable-capacitance diodes are used for RF impedance matching in automatic tuners and transmitters.



 

This is a circuit diagram symbol for a variable-capacitance diode.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.