Contact us

Откроется новое окно Откроется новое окно

What types of op-amps are available?

Op-amps can be divided into two types according to the manufacturing process used:

• Bipolar op-amps

• CMOS op-amps 

Although bipolar op-amps require high input bias current and consume much power, they typically

withstand high voltage.

Conversely, CMOS op amps have low withstand voltage, but feature a small input bias current and low current consumption.

Op-amps can also be categorized into the following types according to their electrical characteristics:
In addition, op-amps can be grouped according to their intended applications:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.