Contact us

Es wird ein neues Fenster geöffnet Es wird ein neues Fenster geöffnet

What is a PIN diode?

A PIN diode is a diode with a near intrinsic semiconductor region (I region) between the typical p-type and n-type regions.
A PIN diode is ideal for automatic gain control (AGC) and transmit/receive switching applications because it can control the series RF resistance via forward current.



This is a circuit diagram symbol for a PIN diode.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.