Contact us

A new window will open A new window will open

How does a load switch IC operate if overcurrent protection is tripped?

When overcurrent protection is tripped, a load switch IC operates in foldback current control mode. Foldback is a current limiting feature. When the load is short-circuited, foldback reduces the output current (IOUT) as the output voltage (VOUT) decreases. When VOUT = 0 V, foldback limits the output current to a level that is internally determined by the load switch IC. When the overcurrent condition has disappeared, VOUT returns to the normal level automatically.
Foldback prevents the heating of a load switch IC in the event of overcurrent conditions. Overcurrent protection is tripped when the output current exceeds the rated level. It is thus intended to provide temporary protection. Be sure to shut down a system so that the overcurrent condition does not last for an extended period of time.

overcurrent protection

Also see the following document and web page for a description of the overcurrent protection function:
To perform a parametric search of load switch ICs with an overcurrent protection function, click:
Other load switch ICs:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.