Characteristics of op-amps (What is the ideal op-amp?)

Generally, it is desirable that amplifiers neither affect the preceding circuit nor be affected by the subsequent circuit. Therefore, amplifiers should have high input impedance and low output impedance.

What is the ideal op-amp?

Op-amps have characteristics close to these requirements. The following compares the ideal and real op-amps:

Fig. 1 Ideal op-amp
Fig. 1 Ideal op-amp

Although there is no such thing as an ideal op-amp, you can assume the ideal op-amp early in the design stage.
However, you should consider the differences between the ideal and real op-amps when you proceed to the detailed design stage.
For example, if the input impedance of an op-amp is low, its input voltage is derived from the input impedance of that op-amp and the output impedance of the preceding device. The low input impedance of an op-amp also affects its feedback loop.
If the output impedance of an op-amp is not zero, its output voltage is derived from the output impedance of that op-amp and the impedance of its load.

In typical applications, however, the input impedance of an op-amp is negligibly large compared with the input impedance of the preceding circuit, and the output impedance is negligibly small compared with the impedance of the subsequent load. Therefore, these impedances usually do not have a significant impact. The same is true of the other parameters shown above.
Take their impacts into consideration when creating a detailed design.

Related Links

The following documents also contain related information:

A new window will open