Contact us

Откроется новое окно Откроется новое окно

How should the power and input signals be sequenced at power-up and power-down?

Generally, a device should be powered up in the following sequence to ensure that the absolute maximum ratings will be met: 1) ground, 2) Vcc, 3) input signals. It is recommended to power down a device in the reverse order.

To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.