Contact us

Откроется новое окно Откроется новое окно

What are the Auto Selection and Manual Selection modes?

The TCK32 Series of load switch ICs (power multiplexers) provide the Auto Selection and Manual Selection modes, which allow selection between two power lines. In Auto Selection mode, the TCK32 Series determines whether VINA and VINB are within the normal voltage range and automatically passes whichever is at a normal input voltage to the output. When both VINA and VINB are within the normal voltage range, VINA is given precedence. In Manual Selection mode, the TCK32 Series selects either VINA or VINB according to the signal applied to the VSEL terminal.

Also see the following document and web page for a description of the Auto Selection and Manual Selection modes:
To perform a parametric search of load switch ICs with Auto Selection and Manual Selection modes, click:
Other load switch ICs:
To Top
·Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant TOSHIBA information and the instructions for the application that Product will be used with or for.