This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
The TCK32 Series of load switch ICs (power multiplexers) provide the Auto Selection and Manual Selection modes, which allow selection between two power lines. In Auto Selection mode, the TCK32 Series determines whether VINA and VINB are within the normal voltage range and automatically passes whichever is at a normal input voltage to the output. When both VINA and VINB are within the normal voltage range, VINA is given precedence. In Manual Selection mode, the TCK32 Series selects either VINA or VINB according to the signal applied to the VSEL terminal.
Also see the following document and web page for a description of the Auto Selection and Manual Selection modes:
To perform a parametric search of load switch ICs with Auto Selection and Manual Selection modes, click:
Other load switch ICs: